This is one of the most common uses, if not the most popular use. While applying tape to surfaces before decorating may seem like a simple task, it is important to utilise the correct techniques. Care should always be taken to avoid any gaps, lines that aren’t straight, or improperly stuck-down tape, as these common errors could lead to issues further down the line.
What is the Difference Between Masking Tape and Painter’s Tape?
In the simplest terms, masking tape and painter’s tape are the same product. However, there are important similarities between the two which makes selecting the right type all the more important. Getting into the specifics, painter’s tape is a sub-type of masking tape.
As a general rule, traditional masking tape is usually less sticky than specialist painter’s tape. By contrast, painter’s tape (often blue tape) is typically used for more specialist applications and for creating high-quality, clean paint lines. It is designed to prevent paint bleed and peel away with ease, whereas masking tape is a much more general-purpose product.
How to Tape a Room Before Painting
The simplest approach to take when preparing a room for painting is that the masking tape should act as a border between the area you want to paint and the rest of the room. In simple terms, once the room has been fully masked, everything within the borders created by the tape needs to be painted.
This includes taping off the top and bottom of the walls (where the wall meets the ceiling and the floor or skirting board, to prevent drips), taping around the door and windows, as well as any non-removable fixtures and fittings like light switches, plug sockets, lights etc. If you are painting a feature wall, make sure to mask it off from the rest of the room too, to provide straight lines between different colours.