Recently searched

    Enclosures

    When talking industrial and electrical, an enclosure is a structure used for storing and protecting components that might otherwise be affected by dirt and moisture, thereby getting damaged. Because of their function, enclosures are generally sturdy to offer more safety to the tools or system they enclose, and they can include a locking system.

    RS provides a wide range of enclosures for your application, catering to diverse industries across the Philippines. From industrial enclosures designed to withstand harsh environments to electrical enclosures for your tools and batteries, you can find the perfect solution for your needs.

    Types of Enclosures

    Understanding the different types of enclosures available can help you choose the best solution for your specific needs.

    Specialized Enclosures

    Specialized enclosures are designed for specific products. For example, Arduino boards have custom Arduino enclosures, while Raspberry Pi cases cater specifically to Raspberry Pi devices. These enclosures are engineered to fit perfectly, ensuring maximum protection and functionality for the specific device.

    General Purpose Enclosures

    General purpose enclosures offer versatility, making them suitable for a wide range of applications. They are commonly made from plastic, metal, or PVC and may feature transparent doors for easy viewing of contents. These enclosures are ideal for various environments and can be customized to meet different requirements. They can be in the form of rack enclosures, which are perfect for housing servers and networking equipment, or floor-standing enclosures that provide ample space for larger industrial components.

    Enclosure Configurations

    When selecting an enclosure for industrial, electrical, or any other application, understanding the different configurations can help ensure you choose the right one for your needs. These are the common enclosure configurations available:

    Floor Standing Enclosure

    Floor standing enclosures are robust, freestanding structures designed to accommodate and organize large electrical components and multiple racks for equipment storage. These enclosures are particularly well-suited for industrial and commercial environments where space and organization are critical. They offer the flexibility to house a variety of equipment, such as servers, control panels, and power distribution units, making them essential for settings like data centers, manufacturing facilities, and power plants.

    Handheld Enclosure

    Handheld enclosures are perfect for portable use, ideal for carrying small devices like batteries, PCBs, or tools like screwdrivers. Their modular design allows storage and protection of various electrical components in a single box. Some handheld enclosures are designed to be waterproof, providing an added layer of protection against moisture, making them suitable for outdoor or harsh environments where safeguarding sensitive electronics from water damage is crucial.

    Wall Mounted Enclosure

    Wall mounted enclosures, also known as wall boxes, are a practical solution for environments where conserving floor space is essential. Designed to be mounted on walls, these enclosures offer a compact yet effective way to store and protect electrical components, making them ideal for both industrial and commercial settings where every square meter of space is valuable.

    Mounting and Installation of Enclosures

    Proper mounting and installation are crucial for the effective use of these protective enclosures. Several accessories and tools are typically needed to ensure a secure and functional installation.

    Mounting Rails

    Mounting rails provide a stable framework for securing components within the enclosure, ensuring that everything stays in place during operation.

    Mounting Plates

    Mounting plates offer a surface for attaching various components inside the enclosure, providing additional stability and organization.

    Brackets, Screws, and Fasteners

    These essential accessories help secure the enclosure to its mounting surface, ensuring that it remains firmly in place.

    Screwdrivers & Drills

    Having the right screwdrivers and drills is essential for the proper assembly and installation of the enclosure, ensuring that all components are securely fastened.

    Measurement and Leveling Tools

    Accurate measurement and leveling tools are vital to ensure that the enclosure is installed correctly, avoiding any potential issues due to misalignment.

    IP Rating for Enclosures

    Most enclosures feature an IP (Ingress Protection) rating which is an international standard used as a measure of the protection offered by the structure against foreign bodies and moisture. IP ratings are made of two digits which indicate the degree of protection on two progressive scales: the first digit indicates the effectiveness of isolation against intrusive bodies, whereas the second digit indicates protection against several moisture agents such as sprays, condensation or strong water jets.

    When buying an enclosure, especially for industrial settings, it’s essential to consider the IP rating. To ensure you select the appropriate rating, take the following factors into account:

    Assess Environmental Conditions

    Evaluate the environment where the enclosure will be used to determine the level of protection required. IP ratings help identify the degree of protection against dust, moisture, and other foreign bodies.

    Application-Specific Requirements

    Consider the specific needs of your application. For instance, waterproof enclosures might be necessary for outdoor installations or environments with high humidity.

    Regulatory and Safety Standards

    Ensure that the enclosure meets local and international regulatory and safety standards, which are particularly important in the Philippines for industrial applications.

    Futureproofing

    Consider long-term use when selecting an enclosure. Choosing a higher IP rated enclosure can provide better protection and adaptability for future changes in your setup.

    Purchasing Enclosures at RS

    RS is your one-stop shop for enclosures in the Philippines. We offer a wide variety of enclosures to protect your equipment in any industrial setting. From durable industrial enclosures to practical rack enclosures, we have what you need. Our selection is designed to ensure the reliability and safety of your equipment in every application.

    Aside from enclosures, we also have other components and equipment available, such as pipes and fittings, cable management tools, labeler tapes, and more. Explore our catalog today and discover the ideal products to meet your specific requirements.

    Make sure to also check out our delivery information to learn about our fast and reliable shipping options nationwide.

    Guides & Articles

    IP Rating Guide

    IP Rating Guide

    This comprehensive guide looks at what IP ratings are, how they’re used and what IP rated products are currently available on the market.

    Read more
    Wall Boxes Guide

    Wall Boxes Guide

    In this complete guide we look at what wall boxes are, what they are used for and the different types available on the market.

    Read more